Product Announcement
Hubbell’s EdgeConnect™ screwless termination straight blade duplex receptacles now offer shorter bridge straps
Installers can terminate receptacles faster and more securely with EdgeConnect™ series devices from Hubbell Wiring Device-Kellems.
These new straight blade duplex receptacles offer shorter bridge straps without ears to eliminate time associated with removing them manually.
EdgeConnect™ Technology devices install faster, with no torque screwdriver needed to secure the termination. Simply insert the wire and activate the color-coded plunger. This reduces wiring time by 65-80%, as quickly as 11 seconds.
Many applications require a condensed mounting strap to fit the device into hard-to-reach places. Previously the ears of the yoke had to be removed before installing the receptacles into tables, hospital head walls, generators, outdoor power distribution units, RACO® Crushed Corner Covers®, or in a prefab shop.
Additionally, shorter straps have the option for a standard opening or threaded screw hole. Both options relieve the user of having to manually remove the auto ground. The threaded hole eliminates the need for an additional nut. Simply screw the device into the application. EdgeConnect™ offers fast termination and trusted durability and premium performance.
Learn more by contacting your Hubbell sales representative, or visit https://www.hubbell.com/wiringdevice-kellems/en/edge-connect.
Austdac is voluntarily notifying all customers and end users of the Austdac Uninterruptible Power Supply (UPS) Type 12/NMH/288 (Part Number UPS12NMH288-1000-B) manufactured between January, 2020 and May, 2024, ("Affected Products"), that some Affected Products may have been fitted with uncertified glands and blanking plugs, and therefore may not meet the requirements of the certificate IECEx TSA 13.0017X issue 5.
Certificate IECEx TSA 13 0017X issue 5 requires that all glands and blanking plugs fitted to the internal Exe enclosure and to the mains cable gland on the main enclosure, be an Exe gland or Exe blanking plug.
Due to a manufacturing process issue, some Affected Products may have been fitted with OSNU and OSNJ series glands, which are not Ex e certified. While these glands have not been marked with the Exe certification mark, our third party supplier has confirmed that the fitted glands meet the requirements of the IECEx certified OS-A2F series Exe gland and, as such, Austdac has no reason to believe that the Affected Products will fail under normal use.
In addition, some Affected Products may have been fitted with a grey nylon blanking plug which is not Exe certified as required by Certificate IECEx TSA 13 0017X issue 5. Austdac notes that the IP rating of the grey nylon blanking plug is IP66 and that the temperature range of the fitted plugs exceeds that of the UPS IECEx certificate rating and the material is rated at UL94 V2.
The glands and blanking plugs are fitted to the Affected Products at the locations shown in Figures 1 and 2 below
Figure 1. Austdac UPS gland plate view (note that correct gland is fitted in this photo)
Manufacturing bill of materials changes have been implemented to ensure that this issue does not recur, and all glands and blanking plugs used in products manufactured after June 1, 2024 use the Exe certified glands and blanking plugs, meeting the requirements of the certificate IECEx TSA 13.0017X issue 5.
While there has been no reported injury, nor has there been any reported equipment or property damage to date, Affected Products may not conform to the certificate IECEx TSA 13.0017X issue 5.
Austdac has developed the following alternative solutions that customers can implement with respect to the Affected Products:
1. Replacement done at time of Affected Product's service. repair or overhaul
Austdac will replace the non-certified glands and blanking plugs fitted to the internal Ex e enclosure and the mains gland with certified glands and blanking plugs when an Affected Product is returned to Austdac for service, repair or overhaul.
2. Rectification at Customer's request
Customers that wish to replace the glands and blanking plugs immediately may return the Affected Product(s) to Austdac for warranty replacement. Alternatively, Austdac will provide a replacement kit containing certified glands and blanking plugs and instructions so that customers can perform a replacement of the glands and plugs on any Affected Product at an Ex competent workshop.
We appreciate your company's help with this important program, and we ask that you please direct any questions or need for further information to Austdac's Customer Service (email: CustomerService@austdac.com.au; telephone: 1800 568 984)
Download Austdac Uninterruptible Power Supply (UPS) Type 12/NMH/288 - Product Advisory Notice